Part Number: CC2500
Other Parts Discussed in Thread: MSP430G2433,
在对CC2500发送sleep命令之后,我们发现它有时候并没有进入sleep状态,这导致我们的产品耗电速度加快。查看芯片手册,发现CC2500没有提供sleep状态的某些反馈查询手段,所以目前无法确定CC2500是否进入sleep状态。以上情况概率性发生,我们将MCU睡眠,而刻意不发送sleep命令,能百分之百复现上述情况。低功耗电流为1.7mA,故此,我们认为芯片未进入sleep状态。想请问,CC2500的sleep命令,是否需要注意某些特定操作步骤或者时序问题。相关代码,我贴在下面。MCU用的MSP430G2433,系统关机之前,采用看门狗复位方式,从mian函数开头进入休眠。
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
IFG1 = 0;
CLK_init();
Port_init();
memset(id, 0xff, sizeof(id));
read_array((unsigned char *) FLASH_ADDRESS, id, sizeof(id));
// If the work mode in flash is empty, just use the default one.
if (FALSE == CheckValidInFlash())
{
restore_saving_data();
}
adc_off();
PWM_Init();
Unit_Init();
SPI_Init();
CC2500_Init();
CC2500_Write_RxADDR();
CC2500_Command(CCxxx0_SPWD); //CC2500 Sleep
if(((P2IN & PRECHARGE_STATE) ==PRECHARGE_STATE)) // no charge battery tonya
{
#if AUTO_TURN_ON_IN_ABNORMAL_SHUTDOWN
if (id[DEVICE_AVOID_ESD] == KEEP_WORKING_AFTER_ABNORMAL_SHUTDOWN_FLAG_OFF)
#endif
{
_BIS_SR(LPM4_bits + GIE); // Enter LPM4 w/interrupt
}
}
else
{
#if DEVICE_LOCK_FUNCTION
id[DEVICE_LOCK_STATE] = UINT_UNLOCK; // Release key lock
#endif
#if AUTO_TURN_ON_IN_ABNORMAL_SHUTDOWN
id[DEVICE_AVOID_ESD] = KEEP_WORKING_AFTER_ABNORMAL_SHUTDOWN_FLAG_OFF;
#endif
id[LOW_POWER_INDICATOR_FLAG] = LOW_POWER_INDICATOR_FLAG_OFF;
__disable_interrupt();
flash_erase( (unsigned int *) FLASH_ADDRESS);
write_array((unsigned char *) FLASH_ADDRESS, id, sizeof(id));
Delay_ms(5);
ChargeFlag=1;
ChargeState = CHARGING_NOT_IN_STATUS;
_BIS_SR(GIE); // Enter interrupt
}
}
void CC2500_Init(void)
{
unsigned char temp;
CSN_ON();
delay_ms(1);
CSN_OFF();
delay_ms(1);
CSN_ON();
delay_ms(1);
CSN_OFF();
SPI_Write(CCxxx0_SRES); //write reset command
CSN_ON();
do{
CC2500_WriteReg(CCxxx0_FSCTRL1, CC2500_Config.FSCTRL1);
CC2500_WriteReg(CCxxx0_FSCTRL0, CC2500_Config.FSCTRL0);
CC2500_WriteReg(CCxxx0_FREQ2, CC2500_Config.FREQ2);
CC2500_WriteReg(CCxxx0_FREQ1, CC2500_Config.FREQ1);
CC2500_WriteReg(CCxxx0_FREQ0, CC2500_Config.FREQ0);
CC2500_WriteReg(CCxxx0_MDMCFG4, CC2500_Config.MDMCFG4);
CC2500_WriteReg(CCxxx0_MDMCFG3, CC2500_Config.MDMCFG3);
CC2500_WriteReg(CCxxx0_MDMCFG2, CC2500_Config.MDMCFG2);
CC2500_WriteReg(CCxxx0_MDMCFG1, CC2500_Config.MDMCFG1);
CC2500_WriteReg(CCxxx0_MDMCFG0, CC2500_Config.MDMCFG0);
CC2500_WriteReg(CCxxx0_CHANNR, CC2500_Config.CHANNR);
CC2500_WriteReg(CCxxx0_DEVIATN, CC2500_Config.DEVIATN);
CC2500_WriteReg(CCxxx0_FREND1, CC2500_Config.FREND1);
CC2500_WriteReg(CCxxx0_FREND0, CC2500_Config.FREND0);
CC2500_WriteReg(CCxxx0_MCSM0 , CC2500_Config.MCSM0 );
CC2500_WriteReg(CCxxx0_FOCCFG, CC2500_Config.FOCCFG);
CC2500_WriteReg(CCxxx0_BSCFG, CC2500_Config.BSCFG);
CC2500_WriteReg(CCxxx0_AGCCTRL2, CC2500_Config.AGCCTRL2);
CC2500_WriteReg(CCxxx0_AGCCTRL1, CC2500_Config.AGCCTRL1);
CC2500_WriteReg(CCxxx0_AGCCTRL0, CC2500_Config.AGCCTRL0);
CC2500_WriteReg(CCxxx0_FSCAL3, CC2500_Config.FSCAL3);
CC2500_WriteReg(CCxxx0_FSCAL2, CC2500_Config.FSCAL2);
CC2500_WriteReg(CCxxx0_FSCAL1, CC2500_Config.FSCAL1);
CC2500_WriteReg(CCxxx0_FSCAL0, CC2500_Config.FSCAL0);
CC2500_WriteReg(CCxxx0_FSTEST, CC2500_Config.FSTEST);
CC2500_WriteReg(CCxxx0_TEST2, CC2500_Config.TEST2);
CC2500_WriteReg(CCxxx0_TEST1, CC2500_Config.TEST1);
CC2500_WriteReg(CCxxx0_TEST0, CC2500_Config.TEST0);
CC2500_WriteReg(CCxxx0_IOCFG2, CC2500_Config.IOCFG2);
CC2500_WriteReg(CCxxx0_IOCFG0, CC2500_Config.IOCFG0);
CC2500_WriteReg(CCxxx0_PKTCTRL1, CC2500_Config.PKTCTRL1);
CC2500_WriteReg(CCxxx0_PKTCTRL0, CC2500_Config.PKTCTRL0);
CC2500_WriteReg(CCxxx0_ADDR, CC2500_Config.ADDR);
CC2500_WriteReg(CCxxx0_PKTLEN, CC2500_Config.PKTLEN);
CC2500_WritePaTable(CCxxx0_PATABLE,PaTabel); //to set output power
temp = CC2500_ReadReg(CCxxx0_FREQ0);
}while(temp!=CC2500_Config.FREQ0);
CC2500_Command(CCxxx0_SFRX);
CC2500_Command(CCxxx0_SFTX);
CC2500_Command(CCxxx0_SIDLE);
}
void CC2500_Command(uint8 cmd)
{
CSN_OFF();
while (MISO_IN);
SPI_Write(cmd);
CSN_ON();
}