Part Number: CC1310
我们在使用HSM进行T/RX间信息传输时,最初使用工程中默认的868MHz的频点,该频点下功能实现正常。
之后根据我方需求,将频率更改至798MHz、808MHz、818MHz、828MHz进行测试,测试结果为818MHz、828MHz下可正常通信,但在798MHz、808MHz下,TX端与RX端无法建立稳定连接。
修改方法:我们参照SmartRF Studio 7中的结果,更改了代码中CMD_FS下的.frequency与CMD_RADIO_SETUP HSM下的.loDivider。
请告诉我们798MHz、808MHz下通信失败的原因。是因为此两处改动并不充分,仍有缺失吗?(例如Overrides for CMD_RADIO_SETUP HSM下的内容需要修改吗?)
// CMD_RADIO_SETUP HSM
rfc_CMD_RADIO_SETUP_t RF_cmdRadioSetup_hsm =
{
.commandNo = CMD_RADIO_SETUP,
.status = 0x0000,
.pNextOp = 0x00000000,
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.mode = 0x05,
.loDivider = 5,
.config.frontEndMode = 0x0,
.config.biasMode = 0x1,
.config.bNoFsPowerUp = 0,
.txPower = 0x0041, //0x23F
.pRegOverride = pOverrides_hsm,
};
// CMD_FS
rfc_CMD_FS_t RF_cmdFs =
{
.commandNo = 0x0803,
.status = 0x0000,
.pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.frequency = 0x0364,
.fractFreq = 0x0000,
.synthConf.bTxMode = 0x0,
.synthConf.refFreq = 0x0,
.__dummy0 = 0x00,
.__dummy1 = 0x00,
.__dummy2 = 0x00,
.__dummy3 = 0x0000,
};