Part Number: CC1101
,我的应用场景是需要收发512字节的数据,我采用了无限收发的模式,也成功实现了两个模块之间的通讯,但是我发现发送接受存在一个丢包,大概只有97%左右的成功率,于是我我现在买了一个SmartRF04EB,安装了SmartRFStio7 想使用这个进行调试一下看下是发送还是接受哪里的问题。但是不知道这个SmartRFStio7 接受发送无限长度应该如何设置。因为按照规格书说明,在发送过程中还要动态调整PKTCTRL0的配置。这个在软件上能够实现吗?因为我看到软件发送接受哪里有一个Infinite的checkbox,但是我点了之后发现并不能正常通讯,所以想了解下这个具体应该如何操作呢?