This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P7: 想用使用Advanced Packet Format模式发送54528字节的数据包

Part Number: CC1352P7

我们使用rfc_CMD_PROP_TX_ADV_t 结构体,目标想要发送54528字节的数据,但现在到了701字节就没办法接收成功,请问可能是什么问题呢?

配置如下:


// CMD_PROP_TX
// Proprietary Mode Transmit Command
rfc_CMD_PROP_TX_ADV_t RF_cmdPropTxAdv_LongRange_400bps =
{
    .commandNo = 0x3803,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bCrcIncSw = 0x0,
    .pktConf.bCrcIncHdr = 0x0,
    .numHdrBits = 0x0,
    .pktLen = 0x0,
    .startConf.bExtTxTrig = 0x0,
    .startConf.inputMode = 0x0,
    .startConf.source = 0x0,
    .preTrigger.triggerType = 0x0,
    .preTrigger.bEnaCmd = 0x0,
    .preTrigger.triggerNo = 0x0,
    .preTrigger.pastTrig = 0x0,
    .preTime = 0x0,
    .syncWord = 0xFE6B2840,
    .pPkt = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};

rfc_CMD_PROP_RX_ADV_t RF_cmdPropRxAdv_LongRange_400bps =
{
    .commandNo = 0x3804,
    .status = 0x0000,
    .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .pktConf.bFsOff = 0x0,
    .pktConf.bRepeatOk = 0x0,
    .pktConf.bRepeatNok = 0x0,
    .pktConf.bUseCrc = 0x1,
    .pktConf.bCrcIncSw = 0x0,
    .pktConf.bCrcIncHdr = 0x0,
    .pktConf.endType = 0x0,
    .pktConf.filterOp = 0x0,
    .rxConf.bAutoFlushIgnored = 0x0,
    .rxConf.bAutoFlushCrcErr = 0x0,
    .rxConf.bIncludeHdr = 0x1,
    .rxConf.bIncludeCrc = 0x0,
    .rxConf.bAppendRssi = 0x0,
    .rxConf.bAppendTimestamp = 0x0,
    .rxConf.bAppendStatus = 0x1,
    .syncWord0 = 0xFE6B2840,
    .syncWord1 = 0x0,
    .maxPktLen = 0x0,
    .hdrConf.numHdrBits = 0x10,
    .hdrConf.lenPos = 0x0,
    .hdrConf.numLenBits = 0x0,
    .addrConf.addrType = 0x0,
    .addrConf.addrSize = 0x0,
    .addrConf.addrPos = 0x0,
    .addrConf.numAddr = 0x0,
    .lenOffset = 2,
    .endTrigger.triggerType = 0x1,
    .endTrigger.bEnaCmd = 0x0,
    .endTrigger.triggerNo = 0x0,
    .endTrigger.pastTrig = 0x0,
    .endTime = 0x00000000,
    .pAddr = 0,
    .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
    .pOutput = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};