This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310:cc1310f32

Part Number: CC1310

编译工程过程中,选用f128的例程去写f32的mcu。更改了.cmd文件中
#define FLASH_BASE 0x0
#define FLASH_SIZE 0x8000 #define RAM_BASE 0x20000000

#define RAM_SIZE 0x4000
后报错:
Command=20 -- addr=0x00001000 -- length=0x00001000
File Loader: 内存写入失败: 状态 0x0102: 目标 flashloader 未能擦除扇区 0。低级函数返回状态 4(作失败)。
can'shcan的GEL:文件:C:\Users\TEMP。LAPTOP-KSREML0U.001\workspace_ccstheia\cc1310f32_0918\Debug\cc1310f32_0918.out: 加载失败。h这是什么原因?还需要哪里修改参数