Part Number: CC1310
CC1310怎么实现1.5Mbps通信@433MHz,需要使用4Fsk调制方式吗,有没有接收器和发射器的相关代码测试下。需要使用TiRTOS吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
// CMD_PROP_RADIO_DIV_SETUP FSK
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup_fsk =
{
.commandNo = 0x3807,
.status = 0x0000,
.pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.modulation.modType = 0x1,
.modulation.deviation = 0x64,
.symbolRate.preScale = 0xF,
.symbolRate.rateWord = 0x8000,
.symbolRate.decimMode = 0x0,
.rxBw = 0x24,
.preamConf.nPreamBytes = 0x4,
.preamConf.preamMode = 0x0,
.formatConf.nSwBits = 0x20,
.formatConf.bBitReversal = 0x0,
.formatConf.bMsbFirst = 0x1,
.formatConf.fecMode = 0x0,
.formatConf.whitenMode = 0x0,
.config.frontEndMode = 0x0,
.config.biasMode = 0x1,
.config.analogCfgMode = 0x0,
.config.bNoFsPowerUp = 0x0,
.txPower = 0xA73F,
.pRegOverride = pOverrides_fsk,
.centerFreq = 0x0364,
.intFreq = 0x8000,
.loDivider = 0x05,
};
这是我的配置,目前可以实现收发,在频谱仪上可以看到带宽大概是600k左右,但是会有丢包,大概10%,可不可以帮忙改善
您好
我们已为CC1312、CC1311和CC1314设备(以及CC135x系列)的1.5 Mbps速率和433 MHz频段制定了初步设置。这些设备包含一个“通用高速”模式补丁,可启用该功能,且支持更为便捷。
对于CC1310,以下线程中存在初步设置(支持有限):
在优化PHY设置时,他们应该参考SWRA682(为CC13x0和CC13x2系列查找新PHY的设置):