This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1125: The issue of transmission power debugging for the CC1125 chip

Part Number: CC1125


Hellow, everyone!

During the power and frequency debugging of CC1125, I encountered the following problems:
Problem 1: When I use the TI tool to configure the power and select the OOK modulation mode, if I change the power at this time, it will show a parameter error. I want to know if the power configuration is related to the modulation mode, as follows:

image.png
Question 2: When I was initializing the CC1125, I found that even though my power was set to 0db by default, the actual test on the spectrum analyzer still seemed to be around 15db. The register configuration and configuration method are as follows:
image.png
 
Question 3: When I was making modifications to the power and frequency, the frequency modification worked properly, but the power modification did not take effect. The method for modifying the power is as follows:
image.png
Note: The working logic of the equipment is as follows:
image.png
The above is the information and questions I can currently provide. If you have any further inquiries, please feel free to contact me. I would be glad to assist you in resolving the current issues. Thank you very much.