CC1312R: Where can I set the frequency of the audio SDK's radio frequency?

Part Number: CC1312R
Other Parts Discussed in Thread: SYSCONFIG

Could you please tell me where to set the radio frequency of the audio SDK? The default frequency band is 868 MHZ. But this wireless frequency band is not available in China.

 

Your previous reply was:

The ROM is programmed during manufactoring. lt's not possible to add something there for the customer.
When you download an example application from the SimpleLink F2 SDK, the linker wil know which objects<e stored in flash and which are stored in ROM.
Please note, due to SW changes, bug fixes etc, newer SDKs use vey little of the ROM sofware.
Cheers,