This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310能否支持4.8kbps的OOK调制模式?

Other Parts Discussed in Thread: CC1310, SMARTRFTM-STUDIO

我是基于Contiki开源的CC1310里的Very-sleepy-demo工程, Radio配置成Prop-mode,我使用Smart RF中生成的4.8kbps ook模式的参数,导入contiki后,发现运行时radio setup出了如下问题:

prop_div_radio_setup: DIV_SETUP wait, CMDSTA=0x00000001,status=0x0002
on: prop_div_radio_setup() failed

prop_div_radio_setup: DIV_SETUP, CMDSTA=0x00000086, status=0x0000
on: prop_div_radio_setup() failed transmit: on() failed

但同样的流程,使用smartrf生成的625bps和contiki里面默认的50kbps参数, RF设置都是正常的。

请问此问题该如何处理? 谢谢

x 出现错误。请重试或与管理员联系。