This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1354P10: MAP_GapInit_cancelConnect() in SDK 8.31 resolves to trap (E7FE) and causes infinite loop when canceling initiating (CC1354P10_6)

Part Number: CC1354P10
Other Parts Discussed in Thread: BLE-STACK

MAP_GapInit_cancelConnect() resolves to trap (E7FE) in SDK 8.31 causing infinite loop during initiating cancel

Environment

  • SDK Version: SimpleLink CC13xx/CC26xx SDK 8.31.00.11

  • Device: CC1354P10

  • Stack Variant: ble5stack_flash / cc1354p10_6

  • Base Example: multi_role

  • Toolchain: TI ARM compiler (CCS)


Problem Description

When operating as Central and performing connection initiation, our application implements a timeout mechanism. Upon timeout, we call the cancel connection procedure (initiator cancel).

However, when this path executes, the system enters an infinite loop inside:

MAP_GapInit_cancelConnect()

The device halts and never returns.


Disassembly Evidence

The function resolves to:

E7FE    b .

This corresponds to a 2-byte infinite branch instruction (trap stub).


Map File Evidence

From the generated .map file:

00060382    00000002     rom_init.o (.text.MAP_GapInit_cancelConnect)

This confirms:

  • MAP_GapInit_cancelConnect is linked from rom_init.o

  • Function size is 2 bytes

  • It matches the trap stub (E7FE)


Expected Behavior

The official examples and stack references indicate that the correct implementation path should call:

GapInit_cancelConnect()

To verify this, we modified rom_init.c as follows:

extern uint8 GapInit_cancelConnect(void);

uint8 MAP_GapInit_cancelConnect(void)
{
#if (HOST_CONFIG & CENTRAL_CFG)
    return GapInit_cancelConnect();
#else
    return bleIncorrectMode;
#endif
}

After this change:

  • The project builds without errors

  • The .map file now shows:

0008262f    GapInit_cancelConnect
  • Cancel connect executes correctly

  • The infinite loop no longer occurs


Observations

  1. GapInit_cancelConnect() exists and links successfully (presumably from OneLib.a).

  2. The default rom_init.c implementation of MAP_GapInit_cancelConnect() appears to be a trap stub.

  3. This trap is reached during a valid central initiating timeout → cancel scenario.


Questions

  1. Why does SDK 8.31 provide a trap implementation for MAP_GapInit_cancelConnect()?

  2. Is this behavior expected only under certain configuration variants?

  3. Is there a required glue-layer variant that should override this stub?

  4. Should this be considered a defect in the cc1354p10_6 ble5stack_flash configuration?

  • 1. This API is meant only for use by the BLE-Stack. The application should always use the GapInit_cancelConnect() API.

    2.  If you use GapInit_cancelConnect you should never see infinite loop behavior.

    3. No. The application should not use MAP_GapInit_cancelConnect().

    4. No.