This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: REV A版本通信问题

Part Number: CC1310

你好,

我在使用SmartRF Studio对测试板1进行测试。测试板1的发射性能(868MHz)与其余测试板相同,RX性能(868MHz)低于其余测试板2~5db。

备注:其余测试板包括LAUNCHXL-CC1310和旧版本的自制测试板,其中的CC1310均为REV B。测试板1为最新自制测试板,误装了REV A 的CC1310。所有自制测试板均按照TI最新参考设计进行设计,且省略了外部LF 晶振。

我的问题:

1.CC1310的版本问题(REV A),是导致TX性能正常,RX性能异常的原因吗?

2.TI何时在中国进行了REV A至REV B的迭代?我在2026年购买的CC1310为REV A版本,是供应商的库存料还是fake芯片?

谢谢。