CC1310: CC1310: 在-20℃设备通信正常,当从-20℃取出来放到室温(25℃)下升温过程中发现个别CC1310死机,目前观察到的死机状态: VDDS供电都正常,DCOUPL无电压,VDDR、VDDR_RF无电压,程序有设置看门狗,但是没复位。

Part Number: CC1310

CC1310在-20℃设备通信正常,当从-20℃取出来放到室温(25℃)下发现个别CC1310死机,目前观察到的死机状态: VDDS供电都正常,DCOUPL无电压,VDDR、VDDR_RF无电压,使用DCDC模式或者全局LDO模式都发现有死机的现象,测试大概100个设备会有2、3个死机的,程序有设置看门狗,但是没复位,。在室温下批量测试设备不会死机,我们的设备有可能会使用在-20环境中,但是从低温切换到室温下个别芯片就进入死机状态了,只能通过对地短接reset管脚或者断电才能恢复正常。怎么解决下呢?