您好~~我想问一下CC2530的那个AD采样,我看了2530的手册,发现他有一个Fullspeed模式,应该是叫全速模式,这个模式是不是就是重复采样的模式呢?如果不是的话,要怎么样实现重复的采样呢?难道只能采样完一次重新开始采样第二次吗?还有一个就是那个带CC2591的这个板子,我看了一下你们的手册介绍,据我的理解和看程序,好像是只用在编译项里添加一个HAL_PA_LNA这个就行了~~但是我看程序里怎么还有一个xHAL_PA_LNA呢?这个是什么意思呢?还是这个协议栈程序是经过别人改造过的协议栈呢?另外还想问一下,带CC2591的模块的RSSI值和不带CC2591的RSSI值是同样的方法得到呢?(我是在那个收到的信息里找打RSSI那一位,然后这个存的是补码,将补码转换成源码就得到RSSI值,这样对吗?)谢谢专家的回答~~