TI 工程师:
你们好。
CC1310如何对FLASH进行读写操作?有没有供用户可以正常使用的一段FLASH空间?
我用FlashSectorErase和FlashProgram函数对0x0001FFD0地址擦除重写时,只有刚烧入程序第一次擦除重写有作用,以后再做同样的操作都返回FAPI_STATUS_FSM_ERROR。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI 工程师:
你们好。
CC1310如何对FLASH进行读写操作?有没有供用户可以正常使用的一段FLASH空间?
我用FlashSectorErase和FlashProgram函数对0x0001FFD0地址擦除重写时,只有刚烧入程序第一次擦除重写有作用,以后再做同样的操作都返回FAPI_STATUS_FSM_ERROR。
你好!
我和你让我参考的例子的写法是一样的,但只能写一次。我用示例中的0x1000地址是不能写的
以下是我的相关代码
#define EASYLINK_DSTADDR_LOCATION 0x0001FFD0
#define EASYLINK_ADDR_SIZE 8
uint8_t dstAddr[EASYLINK_ADDR_SIZE]
ret = FlashProgram(dstAddr, EASYLINK_DSTADDR_LOCATION, EASYLINK_ADDR_SIZE);
if(ret == 0){
status = EasyLink_Status_Success;
}