在对CC2530芯片进行Flash写步骤中,有这样的描述:
1、设置FADDRH:FADDRL为起始地址(这是18位字节地址的16个最高有效位)。
请问这个地址设置后是否能自增,还是在编程4个字节后重新设置下一个地址呢?
4、在20us内对FWDATA进行四次写操作。
请问四次写操作具体是如何写的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
z-stack协议附带。如果是做应用,建议直接使用这个函数,快速满足应用需求
/**************************************************************************************************
* @fn HalFlashWrite
*
* @brief This function writes 'cnt' bytes to the internal flash.
*
* input parameters
*
* @param addr - Valid HAL flash write address: actual addr / 4 and quad-aligned.
* @param buf - Valid buffer space at least as big as 'cnt' X 4.
* @param cnt - Number of 4-byte blocks to write.
*
* output parameters
*
* None.
*
* @return None.
**************************************************************************************************
*/
void HalFlashWrite(uint16 addr, uint8 *buf, uint16 cnt)
{
#if (defined HAL_DMA) && (HAL_DMA == TRUE)
halDMADesc_t *ch = HAL_NV_DMA_GET_DESC();
HAL_DMA_SET_SOURCE(ch, buf);
HAL_DMA_SET_DEST(ch, &FWDATA);
HAL_DMA_SET_VLEN(ch, HAL_DMA_VLEN_USE_LEN);
HAL_DMA_SET_LEN(ch, (cnt * HAL_FLASH_WORD_SIZE));
HAL_DMA_SET_WORD_SIZE(ch, HAL_DMA_WORDSIZE_BYTE);
HAL_DMA_SET_TRIG_MODE(ch, HAL_DMA_TMODE_SINGLE);
HAL_DMA_SET_TRIG_SRC(ch, HAL_DMA_TRIG_FLASH);
HAL_DMA_SET_SRC_INC(ch, HAL_DMA_SRCINC_1);
HAL_DMA_SET_DST_INC(ch, HAL_DMA_DSTINC_0);
// The DMA is to be polled and shall not issue an IRQ upon completion.
HAL_DMA_SET_IRQ(ch, HAL_DMA_IRQMASK_DISABLE);
HAL_DMA_SET_M8( ch, HAL_DMA_M8_USE_8_BITS);
HAL_DMA_SET_PRIORITY(ch, HAL_DMA_PRI_HIGH);
HAL_DMA_CLEAR_IRQ(HAL_NV_DMA_CH);
HAL_DMA_ARM_CH(HAL_NV_DMA_CH);
FADDRL = (uint8)addr;
FADDRH = (uint8)(addr >> 8);
FCTL |= 0x02; // Trigger the DMA writes.
while (FCTL & 0x80); // Wait until writing is done.
#endif
}
所有bank都能读写,是否有特殊用途是跟你的应用有关的。如果你是使用IAR,请了解xcl文件的一些定义
如
-D_ZIGNV_ADDRESS_SPACE_START=(((_NR_OF_BANKS+1)*_FIRST_BANK_ADDR)-0x3800)
-D_ZIGNV_ADDRESS_SPACE_END=(_ZIGNV_ADDRESS_SPACE_START+0x2FFF)
-Z(CODE)ZIGNV_ADDRESS_SPACE=_ZIGNV_ADDRESS_SPACE_START-_ZIGNV_ADDRESS_SPACE_END
那这段空间最好是不要FLASH操作的