This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC112X数据传输模块

Other Parts Discussed in Thread: CC1120, CC1200, TIMAC

您好!我这边需要使用CC1120模块做数据传输,因为后期希望使用其作为串口的收发端使用,且波特率为115200,所以希望使用到CC1120的透明传输模式,寄存器配置使用的是smartRF studio中expert mode中的配置参数,:Bit rate 200kbps,4GFSK,max throughput(868),在实际使用的时候,使用IO直接连接到CC1120的GPIO用于发送数据,当数据的速率是100kbps的时候能够正常的运行,当速率为200kbps的时候,数据接收端不正常。

1,请问一下如何可以让速率达到200kbps。

2,因为到模块不需要一直发送数据,因此在数据不发送的时候,发送端的IO会与串口空闲时一样,保持高电平,但是高电平时间过长会在接收端产生很多的噪音信号。而且还会造成接收端高电平宽度降低(如发送10uS高电平10uS低电平,接收到是6uS高电平14uS低电平),请问怎么解决

3,请问怎么使用CC1120的跳频扩频功能。

  • CC1120的最大速率就是200kbps, SmartRF Studio7下面有推荐配置,CC1200速率会快很多,他们都是窄带系列

    跳频你要自己设计了,TIMAC上做好了星型网跳频,但是针对CC26XX,CC25XX和CC13XX的