Other Parts Discussed in Thread: SIMPLICITI
查看simpliciTI的协议栈里面射频发送的源码,CCA发送这里我有一段代码移植不明白
#define MRFI_CONFIG_GDO0_AS_PAPD_SIGNAL() mrfiSpiWriteReg(IOCFG0, MRFI_GDO_PA_PD) /* For CCA algorithm, we need to know the transition from the RX state to * the TX state. There is no need for SYNC signal in this logic. So we * can re-configure the GDO_0 output from the radio to be PA_PD signal * instead of the SYNC signal. * Since both SYNC and PA_PD are used as falling edge interrupts, we * don't need to reconfigure the MCU input. */ MRFI_CONFIG_GDO0_AS_PAPD_SIGNAL();
把GDOx_CFG[5:0]配置成0x1B,PA_PD。这里我一直不明白,这个功能是否是实现了,自动TX检测发送?发送成功后GDO0会出现电平的翻转
跪求TI技术解答!