各位好,最近在研究cc2530,请问怎么使cc2530运行在不同的功耗模式下,上电后,默认工作在什么模式下呢?怎么改变工作模式呢? 在程序里只是选择了高低频振荡源来自RC振荡器或者晶振,怎么让晶振起震呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
默认工作模式Active/idle mode

请下载Z-STACK,参考hal_sleep.c与HAL_BOARD_INIT(),了解工作模式改变和晶振的操作
/**************************************************************
* mode 0 1 2 3
* PM0 PM1 PM2 PM3
****************************************************************/
#define SET_POWER_MODE(mode) \
do { \
SLEEPCMD &= ~0X03; \
if(mode == 0) { SLEEPCMD &= ~0x03; } \
else if (mode == 3) { SLEEPCMD |= 0x03; } \
else { SLEEPCMD &= ~0x03; SLEEPCMD |= mode; } \
PCON |= 0x01; \
asm("NOP"); \
}while (0)