Other Parts Discussed in Thread: CC1310
你好,
请问哪里可以下载到CC1310在LRM模式下4.8K通信的例程。
RF studio 里面只有625波特率的代码。我们需要用到4.8K的波特率。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LONG 你好
4.8k的LRM,我帮你测好了,你把“smartrf_settings.c" 里面的代码改为我下面这个:
#include<driverlib/rf_mailbox.h>
#include <driverlib/rf_common_cmd.h>
#include <driverlib/rf_prop_cmd.h>
#include <ti/drivers/rf/RF.h>
#include <rf_patches/rf_patch_cpe_lrm.h>
#include <rf_patches/rf_patch_rfe_lrm.h>
#include "untitled.h"
// TI-RTOS RF Mode Object
RF_Mode RF_prop =
{
.rfMode = RF_MODE_PROPRIETARY_SUB_1,
.cpePatchFxn = &rf_patch_cpe_lrm,
.mcePatchFxn = 0,
.rfePatchFxn = &rf_patch_rfe_lrm,
};
// Overrides for CMD_PROP_RADIO_DIV_SETUP
static uint32_t pOverrides[] =
{
// override_use_patch_prop_lrm.xml
// PHY: Use MCE ROM bank 3, RFE RAM patch
MCE_RFE_OVERRIDE(0,3,0,1,0,0),
// override_synth_prop_863_930_div5.xml
// Synth: Set recommended RTRIM to 7
HW_REG_OVERRIDE(0x4038,0x0037),
// Synth: Set Fref to 4 MHz
(uint32_t)0x000684A3,
// Synth: Configure fine calibration setting
HW_REG_OVERRIDE(0x4020,0x7F00),
// Synth: Configure fine calibration setting
HW_REG_OVERRIDE(0x4064,0x0040),
// Synth: Configure fine calibration setting
(uint32_t)0xB1070503,
// Synth: Configure fine calibration setting
(uint32_t)0x05330523,
// Synth: Set loop bandwidth after lock to 20 kHz
(uint32_t)0x0A480583,
// Synth: Set loop bandwidth after lock to 20 kHz
(uint32_t)0x7AB80603,
// Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
ADI_REG_OVERRIDE(1,4,0x9F),
// Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
// Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
(uint32_t)0x02010403,
// Synth: Configure extra PLL filtering
(uint32_t)0x00108463,
// Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
(uint32_t)0x04B00243,
// override_phy_rx_aaf_bw_0xd.xml
// Rx: Set anti-aliasing filter bandwidth to 0xD (in ADI0, set IFAMPCTL3[7:4]=0xD)
ADI_HALFREG_OVERRIDE(0,61,0xF,0xD),
// override_phy_gfsk_rx.xml
// Rx: Set LNA bias current trim offset to 3
(uint32_t)0x00038883,
// Rx: Freeze RSSI on sync found event
HW_REG_OVERRIDE(0x6084,0x35F1),
// override_phy_gfsk_pa_ramp_agc_reflevel_0x1a.xml
// Tx: Enable PA ramping (0x41). Rx: Set AGC reference level to 0x1A.
HW_REG_OVERRIDE(0x6088,0x411A),
// Tx: Configure PA ramping setting
HW_REG_OVERRIDE(0x608C,0x8213),
// override_phy_lrm_rom_dsss8.xml
// PHY: Configure DSSS=8
HW_REG_OVERRIDE(0x505C,0x073C),
// override_phy_rx_rssi_offset_5db.xml
// Rx: Set RSSI offset to adjust reported RSSI by +5 dB
(uint32_t)0x00FB88A3,
// TX power override
// Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
ADI_REG_OVERRIDE(0,12,0xF8),
(uint32_t)0xFFFFFFFF,
};
// CMD_PROP_RADIO_DIV_SETUP
rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
{
.commandNo = 0x3807,
.status = 0x0000,
.pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.modulation.modType = 0x0,
.modulation.deviation = 0x99,
.symbolRate.preScale = 0x6,
.symbolRate.rateWord = 0x4EA4,
.rxBw = 0x26,
.preamConf.nPreamBytes = 0x5,
.preamConf.preamMode = 0x0,
.formatConf.nSwBits = 0x20,
.formatConf.bBitReversal = 0x0,
.formatConf.bMsbFirst = 0x0,
.formatConf.fecMode = 0x8,
.formatConf.whitenMode = 0x0,
.config.frontEndMode = 0x0,
.config.biasMode = 0x1,
.config.analogCfgMode = 0x0,
.config.bNoFsPowerUp = 0x0,
.txPower = 0xA73F,
.pRegOverride = pOverrides,
.centerFreq = 0x0364,
.intFreq = 0x8000,
.loDivider = 0x05,
};
// CMD_FS
rfc_CMD_FS_t RF_cmdFs =
{
.commandNo = 0x0803,
.status = 0x0000,
.pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.frequency = 0x0364,
.fractFreq = 0x0000,
.synthConf.bTxMode = 0x0,
.synthConf.refFreq = 0x0,
.__dummy0 = 0x00,
.__dummy1 = 0x00,
.__dummy2 = 0x00,
.__dummy3 = 0x0000,
};
// CMD_PROP_TX
rfc_CMD_PROP_TX_t RF_cmdPropTx =
{
.commandNo = 0x3801,
.status = 0x0000,
.pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.pktConf.bFsOff = 0x0,
.pktConf.bUseCrc = 0x1,
.pktConf.bVarLen = 0x1,
.pktLen = 0x14, // SET APPLICATION PAYLOAD LENGTH
.syncWord = 0x00000000,
.pPkt = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};
// CMD_PROP_RX
rfc_CMD_PROP_RX_t RF_cmdPropRx =
{
.commandNo = 0x3802,
.status = 0x0000,
.pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
.startTime = 0x00000000,
.startTrigger.triggerType = 0x0,
.startTrigger.bEnaCmd = 0x0,
.startTrigger.triggerNo = 0x0,
.startTrigger.pastTrig = 0x0,
.condition.rule = 0x1,
.condition.nSkip = 0x0,
.pktConf.bFsOff = 0x0,
.pktConf.bRepeatOk = 0x0,
.pktConf.bRepeatNok = 0x0,
.pktConf.bUseCrc = 0x1,
.pktConf.bVarLen = 0x1,
.pktConf.bChkAddress = 0x0,
.pktConf.endType = 0x0,
.pktConf.filterOp = 0x0,
.rxConf.bAutoFlushIgnored = 0x0,
.rxConf.bAutoFlushCrcErr = 0x0,
.rxConf.bIncludeHdr = 0x1,
.rxConf.bIncludeCrc = 0x0,
.rxConf.bAppendRssi = 0x0,
.rxConf.bAppendTimestamp = 0x0,
.rxConf.bAppendStatus = 0x1,
.syncWord = 0x00000000,
.maxPktLen = 0x80, // MAKE SURE DATA ENTRY IS LARGE ENOUGH
.address0 = 0xAA,
.address1 = 0xBB,
.endTrigger.triggerType = 0x1,
.endTrigger.bEnaCmd = 0x0,
.endTrigger.triggerNo = 0x0,
.endTrigger.pastTrig = 0x0,
.endTime = 0x00000000,
.pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
.pOutput = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
};