我想了解WL1835MOD如何做 WIFI与BT的RF TX and RX test,是否可以使用SmartRF Studio 7呢?或是有其他Software可以使用?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
112,
目前smarRF studio不支持Wilink的射频测试。
你能详细说一下你是要单独测试wl1835? 还是你是在一个有host/os的系统里面测试?
BR.az
对的,需要下载bts文件的。
可以用HCItester。http://www.ti.com/tool/WILINK-BT_WIFI-WIRELESS_TOOLS
BR. AZ
������ ���112 说:Hi AZ,
我想确认有关wl1835蓝芽测试的接线.
1.UART只要用到BT_CHI_TX & BT_CHI_RX 2线就好,还是要再加上BT_CHI_CTS & BT_CHI_RTS 共4线?
2.除了wl1835的BT_EN_SOC(pin41) 要enable外,是否还有其它 I/O pin需要enable或接地呢?謝謝
112,
1. 4线、2线都可以。 需要配置一下。如果默认的话,我一般的做法是用2线,然后两端的CTS给拉低电平,就不管什么配置都无敌了。:-)
2. 其他悬空即可。(不要拉高拉低的,容易让芯片进莫名其妙的mode)
BR.AZ