Other Parts Discussed in Thread: CC1310, SIMPLICITI
CC1310 REV A 版本 能否强制在 433MHz 下工作? 请TI FAE帮解答,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC1310, SIMPLICITI
CC1310 REV A 版本 能否强制在 433MHz 下工作? 请TI FAE帮解答,谢谢。
2) Removed limitation on frequency bands supported in CC1310. New frequency bands are supported for the CC1310 from die Rev B and onwards, starting with support for frequency bands in the 430-510 MHz range. This will allow customers to use the same device in a number of markets worldwide. Note that current die Rev A material will still be limited to 863-930 MHz only. SmartRF Studio 2.4.3 or later will detect die Rev A devices and issue an appropriate warning as to the applicable frequency range. Please remember to update SmartRF Studio accordingly.
这部分 是啥意思啊,,,模块还没有寄回。。。
您好。REV A如果强制在433M下使用,性能上会比REV B差在哪里?
看一下置顶帖。如果433MHz,是需要RevB的。
http://www.deyisupport.com/question_answer/wireless_connectivity/f/45/t/124625.aspx
BR.AZ