CC1310 REV A 版本 能否强制在 433MHz 下工作? 请TI FAE帮解答,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
2) Removed limitation on frequency bands supported in CC1310. New frequency bands are supported for the CC1310 from die Rev B and onwards, starting with support for frequency bands in the 430-510 MHz range. This will allow customers to use the same device in a number of markets worldwide. Note that current die Rev A material will still be limited to 863-930 MHz only. SmartRF Studio 2.4.3 or later will detect die Rev A devices and issue an appropriate warning as to the applicable frequency range. Please remember to update SmartRF Studio accordingly.
这部分 是啥意思啊,,,模块还没有寄回。。。
您好。REV A如果强制在433M下使用,性能上会比REV B差在哪里?
看一下置顶帖。如果433MHz,是需要RevB的。
http://www.deyisupport.com/question_answer/wireless_connectivity/f/45/t/124625.aspx
BR.AZ