那是不是说假如我使用多个网络,每个网络里又采用一个发射多个接收的模式,所有的发射模块不会影响,所有接收模块只和它同一网络的发射模块通讯?这个是不是在我采用host模式的时候自己设置的,我的意思是网络分组,和每个网络里主从匹配问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
网络分组是可行的,可以使Hostg工作在不同的频道,但文档也有提到,最少要保持6个通道。所以使用多个网络并不是那么完美,尽管共存可被支持。
(摘自ppw configurator Help) Used RF channels It is generally not recommended to exclude RF channels unless the intention is to avoid a known static interferer, or it is needed for regulatory compliance at the edges of the 2.4 GHz band. The RF channel mask must contain at least 6 channels. It is recommended to spread the included RF channels in frequency to make the network more robust against RF multi-path fading.
Specify which of the 18 available RF channels to use. This affects: