This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在studio的CC1120设置参数中,433M官方给出1.2k,1.2窄带,50k的配置参数?如果想在30k,48,等这些速率中,改如何获得deviation的设置。是否有公式,或者其他的方法获得?
Wenjian,
deviation, RXB, crystal accuracy这些指标都是联动的。
具体你可以学习一下
http://e2e.ti.com/support/wireless_connectivity/w/design_notes/dn005-cc11xx-sensitivity-versus-frequency-offset-and-crystal-accuracy?keyMatch=DN005&tisearch=Search-EN-Everything
如果我配置的话,一般把调制指数放到0.5,供你参考。然后在确定其他的值。
BR. AZ
AZ你好,
非常感谢您的回答,我也查看了您推荐的资料,不过对整个确定过程仍有疑惑,能否用434M,10PPmcrystal accuracy,50kbps给一个简单的推演示例以供学习?
Wenjian
这个涉及到傅里叶变换的特征了,假设是50K的速率,那傅里叶变化后,在频谱上是50K的带宽,因为是FSK或者是GFSK的调制,这两个调制特征是:1和0所代表的频率不一样,所以1代表的频率和0代表的频率需要有一定的间隔,这个间隔就是 deviation,在频谱上可以很明显看到两个分隔的尖峰,那这个间隔deviation为多少比较合适呢?间隔越大,分隔越明显,接收方越容易区别,但是会导致频谱的浪费,占用很大的频谱,所以选一个合适的值比较关键,尽量让0和1代表的频率贴近,但是又不重叠,0和1是有50K带宽的,所以他们间隔25K比较合适,也即所谓的格式,deviation=速率(带宽)/ 2。希望这样解析您可以接收,谢谢!