This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1110数据白化的作用



在CC的系统芯片中都有数据白化功能.whiting的中文件直译为白化,真实的意思应该是数据加噪。

白化处理主要是为了避免在传输过程中出现过长的连续0或1的位流模式。基带处理器需要从接收到的模拟数据信号中判断数据是0还是1,但过长的连续0或1位流会造成问题。因为在接收到的模拟数据信号中并不存在象直流信号中那样的参考点,因此必须依靠接收到的最后几个传输信号进行校正。任何连续的0或1的长序列位流串都可能导致校正失败。因此需要采用数据白化技术对信号进行扰码处理,以大大降低出现长序列0或1位流串的可能性