TI工程师,
对于CC1310 TI-15.4-STACK有如下问题,请帮忙解答一下,谢谢。
我们的产品基于CC1310F128芯片,计划使用TI-15.4-STACK工作在433MHz频率上。但是,通过调查发现协议栈貌似只能配置915MHz和863MHz。请帮忙确认一下如何配置才能支持433MHz?
PS: 我们使用的软件平台为simplelink_cc13x0_sdk_1_00_00_13
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师,
对于CC1310 TI-15.4-STACK有如下问题,请帮忙解答一下,谢谢。
我们的产品基于CC1310F128芯片,计划使用TI-15.4-STACK工作在433MHz频率上。但是,通过调查发现协议栈貌似只能配置915MHz和863MHz。请帮忙确认一下如何配置才能支持433MHz?
PS: 我们使用的软件平台为simplelink_cc13x0_sdk_1_00_00_13
带433的新版本发布了。见http://www.deyisupport.com/question_answer/wireless_connectivity/f/45/t/126881.aspx
BR.AZ
多谢提醒!!!
我已下载最新的SDK,有如下疑问请帮忙确认一下:
1)对于使用CC1310作为coprocessor的方案,是否支持433MHz?若支持,应用程序需要做哪些改动?
2)该版软件是否对芯片的版本有强制要求,如VER A/VER B等。
急盼回复!
Gong Bojian
Bojian Gong 说:多谢提醒!!!
我已下载最新的SDK,有如下疑问请帮忙确认一下:
1)对于使用CC1310作为coprocessor的方案,是否支持433MHz?若支持,应用程�需要做哪些改动?
2)该版软件是否对芯片的版本有强制要求,如VER A/VER B等。
急盼回复!
Gong Bojian
Bojian,
2. 有的,还是要revB.
1. CC1310做coprocessor, 啥意思呀:-)
BR.az
Hi AZ,
感谢帮忙确认!
coprocessor即将cc1310做协处理器外接CPU,已经了解到支持。
谢谢,
Gong Bojian