我们现在的想通过ota的方式来实现程序升级
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC1310现在是支持OAD的,请联系TI的销售或者技术支持找Central Team拿例程
你好,能发我邮箱一份吗,谢谢
jhz1371723247@163.com
您也可以参考链接
这是CC1350的例程,但您可以用相同的方法来在CC1310上来实现。
希望对您有所帮助,谢谢!
您好!能把CC1310升级例程发我一份吗,感谢!
crepse@163.com
请问 Eggsy Pang
这个例子里有这样一段程序
// Supported flash devices
static ExtFlashInfo_t flashInfo[] =
{
{
.manfId = MF_MACRONIX, // Macronics
.devId = 0x15, // MX25R1635F
.deviceSize = 0x200000 // 2 MByte (16 Mbit)
},
{
.manfId = MF_MACRONIX, // Macronics
.devId = 0x14, // MX25R8035F
.deviceSize = 0x100000 // 1 MByte (8 Mbit)
},
{
.manfId = MF_WINBOND, // WinBond
.devId = 0x12, // W25X40CL
.deviceSize = 0x080000 // 512 KByte (4 Mbit)
},
{
.manfId = MF_WINBOND, // WinBond
.devId = 0x11, // W25X20CL
.deviceSize = 0x040000 // 256 KByte (2 Mbit)
},
{
.manfId = 0x0,
.devId = 0x0,
.deviceSize = 0x0
}
};
是不是说1310的外部flash就支持这几种呢?最小的flash就是2M的?