This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于TI的cc2530使用集成balun能量损耗很大的问题

Other Parts Discussed in Thread: CC2530

最近我在cc2530上使用了一块集成的balun,原本是想节省点事,不使用分离元件,以后也方便替换。可是使用后用频谱仪测量后发现有6-7个dB的损耗,调试了很久,还是没有效果,下面是我的使用条件:

方式一:

1、使用过的balun有Johanson的2450BM15A0002(插损1.5dB),Murata的LFB182G45BG2D280(插损1.75dB),但是能量损耗都很大,估计还是PCB的问题

2、双面板,1.0mm厚

3、cc2530与集成balun之间的距离比较近,两元器件引脚之间的距离大约110mil

4、cc2530与集成balun之间的连线使用了差分阻抗200 Ohm的阻抗匹配,线粗8mil

5、balun与天线之间的连线使用了50 Ohm的阻抗匹配

方式二:

1、使用过的balun有Johanson的2450BM15A0002 ,Murata的LFB182G45BG2D280,但是能量损耗都很大,估计还是PCB的问题

2、双面板,1.0mm厚

3、cc2530与集成balun之间的距离拉的非常近,两元器件引脚之间的距离大约0.7mm

4、cc2530与集成balun之间的连线线粗有4mil、5mil、6mil、7mil、8mil、9mil、10mil、12mil、14mil各一个版本,但是都不好,好的损耗6dB,差的7dB

5、balun与天线之间的连线使用了50 Ohm的阻抗匹配

求助各位高手,到底是什么原因有这么大的损耗?如何改进?感激不尽