This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1310的Long range mode模式

Other Parts Discussed in Thread: CC1310

各位TI的大牛们,之前在帖子里面看到说CC1310支持Long range mode模式,当速率为5kbps时,传输距离可以达到20km,这个是真的吗???能否详细的解释一下或者给出相关的说明文档,谢谢啦。。。。

  • 论坛有类似问题,给出了下载地址,请参考这边: http://www.deyisupport.com/question_answer/wireless_connectivity/f/45/t/116730.aspx

  • 谢谢你的回答,我最想问的是那个传输距离20km是不是真的可以达到???如果真的可以达到,那需要多大的发射功率???

  • 货真价实,童叟无欺。我亲自测试的。:-)

    除了强大的链路预算外,但确实是有几个理想条件的:

    1. 够高,地面的反射不会有很大影响。 而且不受地球曲率影响,视距传输,这点很重要。无线信号如果有阻挡的话,衰落会很快。

    2. 干扰小,挪威北部,没啥人的:-),也没啥设备。(其实我挺好奇,4G信号满格)

    空气清新;-)没有pm2.5; 空气湿度也不大,(joking)

    其实你会看到RSSI还在-105dBm的样子。也就是说,还有更远的可能性。(5kbps,SLR 灵敏度为-119dBm)

    BR.AZ