This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1310 rtc晶振问题

Other Parts Discussed in Thread: CC1310, CC2640

在做cc1310设计的时候,想节省电路板空间,想省去32.768k的晶振。请问可以省去吗?之前在论坛里面问过,带ti-rtos操作系统,必须使用rtc时钟。我把电路板上的32.768k晶振去掉,还是可以正常运行。是不是在无外部32.768k晶振的时候,自动切换到内部时钟振荡器上了呢?

  • Bo Lai,

    目前CC1310还没有类似的文档。我找到一篇CC2640的,其实非常类似,可以参考http://www.ti.com/lit/an/swra499b/swra499b.pdf 

    BR.AZ

  • BR.AZ,我看了提供的数据文件,发现对芯片版本有要求,cc2640要求chip version必须在2.3及以上才行。另外,我查到针对cc1310的话,需要Rev B。

    我手里的cc1310是Rev A,我是这么测试的:去掉cc1310的32.768kHz晶振,建了一个最简单工程,一个任务循环控制LED的亮和灭,每次循环都会调用Task_sleep()函数进入睡眠状态。

    这种测试是不是没有用到RTC晶振,所以才可以正常运行。

  • 呵呵,好问题。不知道呀。。。。。你测量一下电流看看?如果电流降到1uA,那就24MHz肯定停了。

    PG2.3@2640和revB@1310才可以支持内部RC是对的。

    BR. AZ