This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
装7.1吧, 离线版的. 另外,你到底是什么专业版? XP不一定支持了.
如下link:
http://software-dl.ti.com/ccs/esd/CCSv7/CCS_7_1_0/exports/CCS7.1.0.00016_win32.zip
If you are using an MSP LaunchPad or a SensorTag you can begin working with these boards without downloading CCS. Visit dev.ti.com to access Cloud-based development tools. Resource Explorer provides instant access to all of the examples, documentation and libraries, CCS Cloud is a cloud-based IDE and PinMux enables you to select your peripherals and generate the pin configuration.
Version 7.1.0.00016 Linux Installation Instructions | System Hardware Requirements | Training Material
Licensing: CCSv7 is now Technology Software Publicly Available (TSPA) compliant. In practice, it does not require a paid license for its use anymore.
Update Status: This release will be available as an update
Internet Explorer users may need to change the extension of the Windows installer to exe after downloading.
This installation program will allow you to select the features of CCS that you want to install and then will download and install just those items. Full zip images 'are available if you have issues with the web installer.' Previous versions are also available. Please see the Linux Host Support CCSv7 and MacOS Host Support CCSv7 pages for device support information as not all devices are supported on these platforms.
Device support on Mac Please note that only microcontroller and connectivity devices are supported on Mac. Processors devices are not support. See MacOS Host Support CCSv7 for more information
4K Display Note if you are using a 4K display the text will auto scale in the installer which makes it very difficult to read the text displayed within the window area and thus not possible to install CCS. It is recommended to disable text scaling or lower the resolution until an updated installer can be created that is compatible with 4K displays.
C55x Users: the C5500 compiler is not installed in CCSv7.x releases, but it is instead available at the CCS App Center, accessible from the View menu in CCS.
With the release of CCSv7 all previous v4, v5 and v6 releases are free of charge. Simply unzip and copy the License File for Older versions into <install dir>/ccs_base/DebugServer/license. Then go to Help -> Code Composer Studio Licensing information and point CCS to this license file. Restart CCS.
When a new release is posted, it may be possible to incrementally update an existing older version of CCS to the newly released version via the CCS Update Manager. Note that this incremental CCS update will only update the IDE components. Also note that not every release will have an incremental update available. More details on the CCS update policy is detailed below:
CCS Update Policy
There are two types of installers:
Release | Build # | Date | Download | Notes | |
7.1.0 | 7.1.0.00016 | Mar 17, 2017 | Web Installers: Windows Linux MacOS |
|
|
7.1.0 | 7.1.0.00015 | Mar 6, 2017 | Web Installers: Windows Linux MacOS |
|
|
7.1.0 | 7.1.0.00014 | Mar 1, 2017 | Web Installers: Windows Linux MacOS |
|
|
7.0.0 | 7.0.0.00043 | Jan 16, 2017 | Web Installers: Windows Linux MacOS |
|
|
7.0.0 | 7.0.0.00042 | Dec 14, 2016 | Web Installers: Windows Linux MacOS |
General Enhancements
Changes
|
It is highly recommended to use the latest version of Code Composer Studio as patches are not provided for older versions.
There are two types of installers:
If you have an issue with the web installer not being able to connect to the internet then please try the off-line installer. If you need to update a computer that does not have internet access then download the offline installer and then transfer it to the computer without access and use the offline installer to update your installation.
Release | Build # | Date | Download | Notes |
6.2.0 | 6.2.0.00050 | Sept 14, 2016 | Web Installers: Windows Linux - 64-bit only MacOS |
|
6.2.0 | 6.2.0.00048 | Aug 31, 2016 | Web Installers: Windows Linux - 64-bit only MacOS |
|
6.1.3 | 6.1.3.00034 | Jul 2, 2016 | Web Installers: Windows Linux |
|
6.1.3 | 6.1.3.00033 | Apr 22, 2016 | Web Installers: Windows Linux |
|
6.1.2 | 6.1.2.00015 | Dec 23, 2015 | Web Installers: Windows Linux |
|
6.1.1 | 6.1.1.00022 | Sept 16, 2015 | Web Installers: Windows Linux |
|
6.1.0 | 6.1.0.00104 | Feb 25, 2015 | Web Installers: Windows Linux |
|
6.0.1 | 6.0.1.00040 | Aug 3, 2014 | Web Installers: Windows Linux |
|
6.0.1 | 6.0.1.00039 | July 22, 2014 | Web Installers: Windows Linux |
|
6.0.0 | 6.0.0.00190 | April 21, 2014 | Web Installers: Windows Linux |
|
It is highly recommended to use the latest version of Code Composer Studio as patches are not provided for older versions.
There are two types of installers:
If you have an issue with the web installer not being able to connect to the internet then please try the off-line installer. If you need to update a computer that does not have internet access then download the offline installer and then transfer it to the computer without access and use the offline installer to update your installation.
Release | Build # | Date | Download | Notes | |
5.5.0 | 5.5.0.00077 | Sep 9, 2013 | Web Installers: Windows Linux Off-line Installers: Use this if the web installer cannot connect to the internet Windows Linux |
|
|
CCSv5.4.x | |||||
5.4.0 | 5.4.0.00091 | May 10, 2013 | Web Installers: Windows Linux Off-line Installers: Use this if the web installer cannot connect to the internet Windows Linux |
|
|
CCSv5.3.x | |||||
5.3.0 | 5.3.0.00090 | Nov 26, 2012 | Web Installers: Windows Linux Off-line Installers: Windows Linux |
|
|
CCSv5.2.x | |||||
5.2.1 | 5.2.1.00018 | July 16, 2012 | Web Installers: Windows Linux Off-line Installers: Windows Linux |
|
|
5.2.0 | 5.2.0.00069 | May 18, 2012 | Off-line Installers: Windows Linux |
|
|
CCSv5.1.x | |||||
5.1.1 | 5.1.1.00031 Windows 5.1.1.00033 Linux |
February 16, 2012 February 27, 2012 |
Windows (offline installer) 1200MB |
|
|
5.1.0 | 5.1.0.09000 | November 3, 2011 |
Windows (offline installer) 1200MB Linux (offline installer) 1100MB |
|
|
CCSv5.0.x (LIMITED DISTRIBUTION) | |||||
5.0.3 | 5.0.3.00028 | June 27, 2011 |
|
||
5.0.2 | 5.0.2.00006 | February 23, 2011 |
|
||
5.0.1 | 5.0.1.00036 | January 24, 2011 |
|
||
5.0.0 | 5.0.0.00095 | October 25, 2010 |
|
This page provides access to current and past download images for Code Composer Studio. The latest link will always be at the top but you can use the other links to download specific versions. For each version are two CCS images that can be downloaded, DVD image and Microcontroller Core. The DVD image is what you get when you buy CCS regardless of which license type purchased and the Microcontroller Core version is the code size limited tool. For updates to BIOS, IPC, XDCtools please go here.
Unless you want code size limited tools then download the full DVD image.
Requirements to Download: You will need a my.TI login to download CCS. If you don't already have one you will be given the opportunity to create one on the login screen. The other thing you will go through when you download CCS is US Export control screening, a questionnaire will appear with some questions that need to be answered. If approved the system will email you the download link. If you are an IE8 user make sure to say "No" to the prompt if you want to view secure content only.
Notice to Windows 7 / 64 bits users: CCSv4.x releases have a known drawing issue on the Project Build properties that can only be partially solved by a patch to the SWT component. Therefore it is recommended to use CCSv5.1 for this OS. For details please check this forum thread
Latest production image is 4.2.4.00033.
DVD (Full Tools) | FREE CODE SIZE LIMITED TOOLS | |||||
---|---|---|---|---|---|---|
|
|
|||||
Getting a License: You need a license to use CCS. There are many types of licenses for CCS. The licensing topic goes into more detail on the options available. The activation topic walks through the process of activating a license. If you are using the MCU Core download it will automatically generate a license on installation and no user action is required. If you have any issues with license file generation please contact: ccs_license_file_help@list.ti.com.
Stellaris: Stellaris Support is available in CCSv4.1 and later. The Stellaris Support in CCS topic describes the status of Stellaris support in CCS.
Release | Build # | Date | Download | Release Notes | Comments | ||
CCSv4.2.x | |||||||
4.2.5 | 4.2.5.00005 | Dec 20, 2011 | Patch only | Patch only | Patch | Release Notes |
|
4.2.4 | 4.2.4.00033 | Jul 18, 2011 | DVD image | Code Size Limited | Patch | Release Notes |
|
4.2.3 | 4.2.3.00004 | Mar 30, 2011 | DVD image | Code Size Limited | Patch | Release Notes | Added support for MSP430 FR57xx, G2xx3, and for low power mode. |
4.2.2 | 4.2.2.00033 | Mar 7, 2011 | DVD image | Code Size Limited | n/a | Release notes |
|
4.2.1 | 4.2.1.00004 | November 30, 2010 | DVD image | Code Size Limited | Patch | Release notes | New MSP430 device support |
4.2.0 | 4.2.0.10018 | November 5, 2010 | DVD image | Code Size Limited | Patch | Release notes | 4.2.0.10017 & 4.2.0.10018 are the same |
CCSv4.1.x | |||||||
4.1.3 | 4.1.3.00038 | July 29, 2010 | DVD image | Code Size Limited | Patch | Release notes | 2 fixes have been added since the first posting of 4.1.3 build 34, build 38 includes a fix for the ROV view not working and for problems when using the RTSC platform wizard |
4.1.2 | 4.1.2.00027 | April 13, 2010 | DVD image | Code Size Limited | Patch | Release notes | Last release with Spectrum Digital XDS560R support |
4.1.1 | 4.1.1.00014 | February 24, 2010 | DVD image | Code Size Limited | Release notes | MSP430 Users: There is a known issue with using the MSP430 Debugger Options (SDSCM00035406). To resolve this issue, copy the 'PropertiesDB.xml' file in this zip into <INSTALL DIR>\DebugServer\propertyDB | |
4.1.0 | 4.1.0.02006 | January 18, 2010 | DVD image | Code Size Limited | Release notes |
|
|
CCSv4.0.x | |||||||
4.0.2 | 4.0.2.01003 | October 30, 2009 | DVD image | Code Size Limited | |||
4.0.1 | 4.0.1.01001 | September 10, 2009 | DVD image | Code Size Limited | Initial v4 DVD image | ||
4.0.0 | 4.0.0.16002 | July 20, 2009 | DVD image | Code Size Limited | Initial v4 download |
Full images for these releases are not available for download.
Major changes in this release stream include support for C64x+ processors, the DaVinci family and some ARM based processors.