CC1101,用 SmartRF Studio 7 生成寄存器配置,默认同步字,发射端和接收端可以通信;但是将同步字设置0x0000和0xffff,就不行了,接收端无法收到数据。请问下 各位前辈,这是为什么?可以怎样解决?CC1101的同步字有什么讲究?谢谢了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
维基百科上对同步字的表述如下:
In computer networks, a syncword, sync character, sync sequence or preamble is used to synchronize a data transmission by indicating the end of header information and the start of data. The syncword is a known sequence of data used to identify the start of a frame, and is also called reference signal or midamble in wireless communications.
你把同步字设置成0x0000或0xFFFF,就起不到同步的作用了。