This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问CC1101支持IEEE802.15.4吗?

Other Parts Discussed in Thread: CC1101, SIMPLICITI

datasheet上没有提到,想确认一下,谢谢各位

  • CC1101支持IEEE802.15.4中的FSK调制方式,但是不支持DSSS。

    你可以参考E2E中BU的回复,

    http://e2e.ti.com/support/wireless_connectivity/proprietary_sub_1_ghz_simpliciti/f/156/t/170010?tisearch=e2e-quicksearch&keymatch=cc1101%20802.15.4

    摘录如下:

    The CC1101 is compatible with the IEEE802.15.4g standard (Mandatory mode, FSK 50 kbps). The IEEE802.15.4g is a PHY amendment to the IEEE802.15.4-2006 standard to provide a global standard that facilitates very large scale process control applications such as the utility smart-grid network capable of supporting large, geographically diverse networks with minimal infrastructure, with potentially millions of fixed endpoints.IEEE802.15.4-2006 specifies the use of DSSS which CC1101 does not support, also there are a very limited number sub-1GHz channels defined.

    The IEEE802.15.4g is an amendment to the 15.4 specification, specifying e.g. more sub-1GHz bands to be used. CC1101 supports the mandatory mode (50 kbps, FSK)  in the 15.4g spec.