This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

单发单收模式,当发射端信号不好,或受到干扰后,CC1101永远接收不到数据了,如何解决

Other Parts Discussed in Thread: CC1310

使用条件:

1、单发,单收。GDO2 中断输出接收。接收端收完一包(60字节)后切换到接收状态继续收。发送端5秒发一次.

发生以下两种情况时,接收端永远收不到数据了。

1、受到干扰。

2、发射端信号不好(离的太远)

后来人为制造发射端信号不稳,比如,发送端发送数据一半的时候断电,然后重启发送端继续发送,此时接收端永远收不到数据了,用示波器测量GDO2(配置为0X07)与GDO0(配置为0x06)也一直测不到信号。

请问如何解决此问题。

配置如下:、

code RF_SETTINGS rfSettings = {
    0x00,
    0x0B,   // FSCTRL1   Frequency synthesizer control.
    0x00,   // FSCTRL0   Frequency synthesizer control.
    0x10,   // FREQ2     Frequency control word, high byte.        // 432.4999M
    0xA2,   // FREQ1     Frequency control word, middle byte.    // 432.4999M
    0x76,   // FREQ0     Frequency control word, low byte.        // 432.4999M
    0xF6,   // MDMCFG4   Modem configuration.                    // 2.4K
    0x83,   // MDMCFG3   Modem configuration.                    // 2.4K
    0x13,   // MDMCFG2   Modem configuration.                    // 步进200kHz
    0x22,   // MDMCFG1   Modem configuration.                    // 步进200kHz
    0xF8,   // MDMCFG0   Modem configuration.                    // 步进200kHz

    0x00,   // CHANNR    Channel number.                        // 频道
    0x00,   // DEVIATN   Modem deviation setting (when FSK modulation is enabled).
    0xB6,   // FREND1    Front end RX configuration.
    0x10,   // FREND0    Front end RX configuration.
    0x18,   // MCSM0     Main Radio Control State Machine configuration.
    0x1D,   // FOCCFG    Frequency Offset Compensation Configuration.
    0x1C,   // BSCFG     Bit synchronization Configuration.
    0xC7,   // AGCCTRL2  AGC control.
    0x00,   // AGCCTRL1  AGC control.
    0xB2,   // AGCCTRL0  AGC control.

    0xEA,   // FSCAL3    Frequency synthesizer calibration.
    0x0A,   // FSCAL2    Frequency synthesizer calibration.
    0x00,   // FSCAL1    Frequency synthesizer calibration.
    0x11,   // FSCAL0    Frequency synthesizer calibration.
    0x59,   // FSTEST    Frequency synthesizer calibration.
    0x88,   // TEST2     Various test settings.
    0x31,   // TEST1     Various test settings.
    0x0B,   // TEST0     Various test settings.
    0x07,   // IOCFG2    GDO2 output pin configuration.            // GDO2设置
    0x06,   // IOCFG0D   GDO0 output pin configuration. Refer to SmartRF?Studio User Manual for detailed pseudo register explanation.// GDO0设置

    0x0c,   // PKTCTRL1  Packet automation control.                // 设置地址过滤用的
    0x05,   // PKTCTRL0  Packet automation control.                // 设置数据白化 CRC校验 数据包模式
    0xa1,   // ADDR      Device address.                        // 设置地址
    0x40    // PKTLEN    Packet length.                            // 数据包长度
};