This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC1101低功耗电流问题

Other Parts Discussed in Thread: CC1101

请教各位大神,CC1101    433M,进入低功耗,处于接收模式,如果接收到有另一个CC1101发来的数据就唤醒,那么,低功耗时,电流最小能达到多少?低功耗时,还要能接收数据。

  • 你可以看一下数据手册中的Figure 13: Simplified State Diagram,了解一下CC1101的各个状态,及它们之间的转换关系

    需要明确的一点时,当CC1101进入低功耗(sleep)时,是无法接收数据的,必须在CC1101处于receive mode的时候,才可以接收数据

    针对你的需求,可以考虑WOR(wake on radio)模式,CC1101大部分时间处于接收状态,周期性的唤醒进入rx模式侦听

    这种工作状态下的平均工作电流与你设定定的WOR interval有关。

    关于WOR,可以查看数据手册19.5  Wake On Radio (WOR) 

  • CC1101接收模式,不接收数据的时候,功耗20MA,是否正常?参考各种资料,WOR也没设置成功,现在我想知道,如果设置成功了,从休眠模式唤醒后功耗是多大,是否能满足我的要求,非常感谢!

  • 你的通信数据不多吧?另外cc1101接收或者发送工作电流还是很大的。

    休眠模式唤醒后可以设置为接收或者发送状态,这时候工作电流比较大。

  • 关于功耗您可以参考http://www.ti.com.cn/cn/lit/ds/symlink/cc1101.pdf的

    Table 4: Current Consumption

    表内所有测量结果均使用CC1101EM参考设计获得

  • 别的公司做的一款产品,待机时,还能正常收发数据,待机功耗只有2.45MA,而且是稳定电流,表示很惊讶,能做到这样?