This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310 SPI

Other Parts Discussed in Thread: CC1310

Hi,

我想将CC1310和传感器进行SPI通信,所以我将SPI做了如下配置:

 SPI_init();
    SPI_Params_init(&SPIparams);
    SPIparams.bitRate     = 4000000;
    SPIparams.frameFormat = SPI_POL0_PHA1;
    SPIparams.mode        = SPI_MASTER;
   
    // Configure the transaction
    transaction.txBuf =  AS393_TxBuffer;
    transaction.rxBuf =  AS393_RxBuffer;
    
    SPIhandle = SPI_open(Board_SPI0, &SPIparams);
    if (SPIhandle == NULL) {
      // System_abort("Error initializing SPI\n");
      asm("nop");
    }
    else {
      asm("nop");
       //System_printf("SPI initialized\n");
    }

,这个配置我看了是在时钟下降沿的时候发送数据的,我现在想让时钟在上升沿发送数据改怎么设置呢?frameFormat里面的几项是什么意思呢?

谢谢!

  • typedef enum SPI_FrameFormat_ {
    SPI_POL0_PHA0 = 0, /*!< SPI mode Polarity 0 Phase 0 */
    SPI_POL0_PHA1 = 1, /*!< SPI mode Polarity 0 Phase 1 */
    SPI_POL1_PHA0 = 2, /*!< SPI mode Polarity 1 Phase 0 */
    SPI_POL1_PHA1 = 3, /*!< SPI mode Polarity 1 Phase 1 */
    SPI_TI = 4, /*!< TI mode (not supported on all
    implementations) */
    SPI_MW = 5 /*!< Micro-wire mode (not supported on all
    implementations) */
    } SPI_FrameFormat;

  • 可以详细阅读TRM文档的20.4.4.2 Motorola SPI Frame Format开始的几个章节了解。