This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS3705应用的一些相关问题

Other Parts Discussed in Thread: TMS3705

你好:

最近在使用TMS3705制作RFID读基站,实现标签读功能。目前使用的是TMS3705数据手册中的典型应用电路,有以下问题需要请教:

1)TMS3705为半双工读写,如果应用只读模式,是否可以读取全双工模式的标签芯片?

2)在TMS3705的TXCT端输入50ms低电平,然后一直为高电平触发一次默认模式读取,在低电平初期SCIO输出的天线诊断字节的数据格式和时序是什么?

3)通过示波器检测的诊断字节为全高(即0xff)是对的吗?

4)天线使用的是自己缠绕的线圈,直流电阻8Ω。发现在感应范围内没有标签时,也会在TXCT低电平结束高电平约3ms后返回一些数据,按照数据手册的状态跳转不应该是没有反馈吗?

5)触发一次默认读取应反馈的是ISO11784卡中的什么内容?

谢谢!