请教一下,我现在设计一款CC1310+PA(sky66115-11) 433MHz的电路,通过Smart RF Stdio软件测试硬件电路没有问题,但是软件除了配置对应管脚映射外怎么设置为单端模式?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
z这个需要配合你的原理图连接来配置如下的参数,然后导出到你的软件里的RF setting文件里面。
可以参考附件文档:swra528_CC1310 Skyworks 433MHz PA Reference Design.pdf
您好,我还有两个问题:
1、因为发射和接收配置的模式不一样,如下图所示,那么我该怎么导出配置文件?而且我的软件协议里面是无法控制收发的
2、TI15.4的demo程序collector->board_palna.c中,有一个函数void Board_Palna_initialize(uint32_t hgm),来配置cc1190的管脚映射。那么sky66115-11应该如何映射管脚呢?
附上函数
void Board_Palna_initialize(uint32_t hgm)
{
if (hgm)
{
CC13x0_LAUNCHXL_rfDisableCallback();
if (!palnaPinHandle)
{
/* Open PA/LNA PIN driver */
palnaPinHandle = PIN_open(&palnaPinState, palnaPinTable);
/* Set IO muxing for RFC GPOs */
PINCC26XX_setMux(palnaPinHandle, Board_CC1190_LNA, IOC_PORT_RFC_GPO0);
PINCC26XX_setMux(palnaPinHandle, Board_CC1190_PA, IOC_PORT_RFC_GPO1);
}
PIN_setOutputValue(palnaPinHandle, Board_CC1190_HGM, (hgm & 1));
}
}
你现在就是在用TI15.4 stack吗?
如果easy link的话,我们是建议客户发射和接受分别调用不同的settings的。
BR. AZ