请问为什么有些1310的例程上并没有看到.cfg文件,那我应该如何看工程中的配置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
/*
* ======== ccfg.c ========
* Customer Configuration for CC26xx and CC13xx devices. This file is used to
* configure Boot ROM, start-up code, and SW radio behaviour.
*
* By default, driverlib startup_files/ccfg.c settings are used. However, if
* changes are required there are two means to do so:
*
* 1. Remove this file and copy driverlib's startup_files/ccfg.c file in
* its place. Make all changes to the file. Changes made are local to
* the project and will not affect other projects.
*
* 2. Perform changes to driverlib startup_files/ccfg.c file. Changes
* made to this file will be applied to all projects. This file must
* remain unmodified.
*/
C:\ti\simplelink_cc13x0_sdk_1_60_00_21\source\ti\devices\cc13x0\startup_files
您指的是哪个工程?