我的代码功能如下:
串口收到配置数据,写入到NVS,如果非配置数据,直接通过RF发送出去。
现在的问题是:串口收到配置数据写入到NVS中,写入能成功,复位后,代码卡死在easylink初始化中。
uart配置:
UART_Handle uart0_handle;//全局变量
UART_Params_init(&uartParams);
uartParams.readMode = UART_MODE_CALLBACK;
uartParams.readCallback = Uart_ReadCallback;
uartParams.writeCallback = Uart_WriteCallback;
uartParams.writeMode = UART_MODE_CALLBACK;
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.baudRate = 9600;
uart0_handle = UART_open(Board_UART0, &uartParams);
if (uart0_handle == NULL) {
System_abort("Error opening the UART");
}
main函数:
int main(void)
{
unsigned char i;
/* Call board init functions */
Board_initGeneral();
// Board_initI2C();
// Board_initSPI();
Board_initUART();
// Board_initWatchdog();
/* Construct heartBeat Task thread */
Task_Params_init(&taskParams);
taskParams.arg0 = 1000000 / Clock_tickPeriod;
taskParams.stackSize = TASKSTACKSIZE;
taskParams.stack = &task0Stack;
Task_construct(&task0Struct, (Task_FuncPtr)echoFxn, &taskParams, NULL);
/* Confirming the sector size on this device is 4096 */
if (FlashSectorSizeGet() != 4096) {
System_abort("Oops! The sector size is not 4096");
}
NVS_init();
nvsHandle = NVS_open(CC1310DK_7XD_NVS1F000, NULL);
for(i=0;i <16;i++)
custom_falsh_write_buffer[i]=1;
/* + 1 to make sure to write the '\0' character */
strSize = strlen(custom_falsh_write_buffer) + 1;
/* make sure the buffer size is a multiple of 4 */
strSize = (strSize + 4) & 0xFFFFFFFFC;
for(i=0;i <16;i++)
custom_falsh_write_buffer[i]=NULL;
status = NVS_write(nvsHandle, 0, custom_falsh_write_buffer, strSize, NVS_WRITE_ERASE | NVS_WRITE_VALIDATE);
if (status != NVS_SOK) {
System_abort("NVS_write failed");
}
status = NVS_read(nvsHandle, 0, custom_falsh_read_buffer, MYBUFFERSIZE);
if (status != NVS_SOK) {
System_abort("NVS_read failed");
}
/* Open LED pins */
ledPinHandle = PIN_open(&ledPinState, pinTable);
if(!ledPinHandle) {
System_abort("Error initializing board LED pins\n");
}
PIN_setOutputValue(ledPinHandle, Uart_Tx_LED, 1);
PIN_setOutputValue(ledPinHandle, Uart_Rx_LED, 1);
cc1190PinHandle = PIN_open(&cc1190PinState, cc1190pinTable);
if(!cc1190PinHandle) {
System_abort("Error initializing board cc1190 pins\n");
}
PIN_setOutputValue(cc1190PinHandle, CC1190PAEN, 0);
PIN_setOutputValue(cc1190PinHandle, CC1190LNAEN, 0);
PIN_setOutputValue(cc1190PinHandle, CC1190HGM, 0);
System_printf("Starting the example\nSystem provider is set to SysMin. "
"Halt the target to view any SysMin contents in ROV.\n");
/* SysMin will only print to the console when you call flush or exit */
System_flush();
/* Start BIOS */
BIOS_start();
return (0);
}
串口写flash代码如下:
case 0x20:
status = NVS_read(nvsHandle, 0, custom_falsh_write_buffer, MYBUFFERSIZE);
if (status != NVS_SOK) {
System_abort("NVS_read failed");
}
custom_falsh_write_buffer[0] = 0X55;
custom_falsh_write_buffer[3] = UART_Rx_Buff[4];
//write
status = NVS_write(nvsHandle, 0, custom_falsh_write_buffer, strSize, NVS_WRITE_ERASE | NVS_WRITE_VALIDATE);
if (status != NVS_SOK) {
System_abort("NVS_write failed");
}
//read
status = NVS_read(nvsHandle, 0, custom_falsh_read_buffer, MYBUFFERSIZE);
NVS_close(nvsHandle);
if (status != NVS_SOK) {
System_abort("NVS_read failed");
}
read_buff_temp[1] = custom_falsh_read_buffer[3];
read_buff_temp[0] = 0x20;
UART_write(uart0_handle, read_buff_temp, 2);
break;
如果不通过uart收到配置数据,写入到flash,正常透传是没问题。
我怀疑是串口收到数据写入到flash出的问题。
NVS配置是:
char myCopyBlock[4096];
const NVSCC26XX_HWAttrs nvsCC26xxHWAttrs[CC1310DK_7XD_NVSCOUNT] = {
{
.block = (void *)(0x1d000 - 4096), // Flash sector to use is 4096 of flash on a 128K part
.blockSize = 4096,
.copyBlock = myCopyBlock,
.isRam = true
}
};
请TI工程师帮我看看有什么问题。