1、板子的底层管脚更改已经完成,对应到了我自己的板子
2、LaunchPad的easylink例程是基于7*7的,现在要将其迁移到4*4的芯片上,要改哪些东西
3、接收端还是使用LaunchPad板子接收
4、频段等通信参数未做更改
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、板子的底层管脚更改已经完成,对应到了我自己的板子
2、LaunchPad的easylink例程是基于7*7的,现在要将其迁移到4*4的芯片上,要改哪些东西
3、接收端还是使用LaunchPad板子接收
4、频段等通信参数未做更改
user5065507 说:您好,我看了这些帖子,他们的问题与我遇到的很不一样
1、我这边移植过后编译是正确的。
2、程序下载之后程序运行正常,串口、GPIO等都工作正常。
3、现在存在的情况是,发送端发送了,但是接收端没有接收到。
4、我把移植前的程序下载到launchPad中作为发送端,接收端却又是可以正常接收的。
5、应该是我在移植过程中没有弄明白对于通信部分,应该做的那些更改?或者是说对于easylink.c或者easylink.h需要做哪些更改?我没有弄明白造成了移植后数据收发不通的现象,
谢谢
射频前端的option用的是哪一个?ID?XS?IS?XD?
BR. AZ