This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310复位

Other Parts Discussed in Thread: CC1310

请问,CC1310 低电,是否回导致不停的复位?复位电压是多少?

  • CC1310的供电范围:1.8 ~ 3.8 V 如果低于最小值可能引起复位
  • 你好:
    请教您一下CC1310的几个复位原因,SysCtrlResetSourceGet()获得复位原因有8个,
    1、RSTSRC_PWR_ON 是上电复位 2、RSTSRC_PIN_RESET 是rst管脚复位 3、RSTSRC_WAKEUP_FROM_SHUTDOWN 是从shutdown唤醒
    请问 RSTSRC_VDDS_LOSS RSTSRC_VDDR_LOSS RSTSRC_CLK_LOSS RSTSRC_SYSRESET RSTSRC_WARMRESET 这5个复位分别是什么原因呢?
    谢谢!!
  • 电源电压复位,时钟丢失复位,软件复位等
  • 完整resetsource有如下:
    RSTSRC_PWR_ON
    RSTSRC_PIN_RESET
    RSTSRC_VDDS_LOSS
    RSTSRC_VDD_LOSS
    RSTSRC_VDDR_LOSS
    RSTSRC_CLK_LOSS
    RSTSRC_SYSRESET
    RSTSRC_WARMRESET
    RSTSRC_WAKEUP_FROM_SHUTDOWN
    直接看字面意思,比如RSTSRC_SYSRESET是system reset,RSTSRC_WARMRESET是warm reset
  • 电压低到一定程度会先触发BOR(Brown Out Detector)来进行保护

    Lowering the supply voltage below the BOD threshold between two recharge periods while in STANDBY may cause the BOD to lock the device upon wakeup until a Reset/POR releases it.

    To avoid this, it is recommended that STANDBY mode is avoided if there is a risk that the supply voltage (VDDS) may drop below the specified operating voltage range. For the same reason, it is also good practice to ensure that a power cycling operation, such as a battery replacement, triggers a Power-on-reset by ensuring that the VDDS decoupling network is fully depleted before applying supply voltage again (for example, inserting new batteries). This restriction does not apply to CC1310 die rev B or later.
  • 在电池电压低时,我如何确保此次的发射(13dBm)工作能够正常完成,且不会发生因为“Brown out detect on VDDS”?