This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC111x 关于USART的UART和SPI选择



在CC111x中,USART有UART和SPI两种模式,请问:

一、在同一个USART外设中,UART和SPI模块可以同时运行使用吗?

二、如上述问题可行,那么在引脚不冲突的情况下,USART0和USART1中的UART0、SPI0、UART1、SPI1 4个外设可以同时运行使用吗?