Hello,Everyone I have a qustion about the Project "Home Automation Sample Light and Home Automation Sample Switch.
The Chip is CC2530.
Now,I can use the Terminal in the PC then send a message to the Coordinator(Sample Switch) and then my End Devie(Sample Light) can turn on the light.
But now,for example,I want to use the Router to contorl more than five Endpoint.
And then in the file "HomeAutomation\SampleSwitch\Source\zcl_samplesw.h" , I saw the "#define SAMPLESW_ENDPOINT 12" .
So I find some data about the ENDPOINT , but I only find the EndPoint 's use 1-240.
If I want to use the Project of Home Automation ,how many numbers of EndPoint(1-240) can I use in the Home Automation?
Thanks a lot!.