I want to use the SBL to download my project to the CC2530. But,my project is based on Z-STACK 2.3.1,and the SBL-tools is in Z-STACK2.5.1a.Then,I use the Z-STACK 2.5.1a open the project and make the bin-file,but,when i use the SBDemo download the bin-file,it doesnt work.I dont know if should i upgrading the Z-STACK, Can you give me some suggestions,thanks a lot!
Best regards!
Jake