This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请问CC85xx系列可以实现心音(低频)的无线传输吗?
你好!
人的心率每分钟60次,也就是一秒钟1HZ,CC85XX规格是20~20KHz,不能直接传输传输。
您好,首先感谢你的回答,不过我问的是心音,不是心律。。。心音的低频段在20到200左右,但我不知道能不能用CC85XX,而且目前此款芯片貌似没有开发板。。。
Hi,Jacky Hou
CC85XX可以支持低至20Hz的频率,因此您这个频率范围是可以无线传输。开发板Ti有CC8520的,您可以向TI订购,不过挺贵。
恩,如果有的话我倒是挺感兴趣的,您说的挺贵我想打听下大概的价位是多少呢?
不用啦,我买了是 1200 ,现在已经国产化了!!你会动手的话我有开发成功的 PCB (文件)你可以做,CC8530 是目前市场上专门处理音频数据流最好的无线IC比 24z01 的好很多很多