最近买了一套CC1120的官方开发版,通过smart RF调试,没有看到cc和交织的相关配置,可是cc1101看到芯片是支持的,是否CC1120硬件不支持CC和交织呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC112支持前导码校验以及CRC校验。
CRC is a checksum used to detect bit errors in the receive message to be able to discard packets without valid data. Can disable everything and use as pass through receiver. If the receive signal qualifiers are integrated in the radio, false error check can be done without MCU intervention. Put MCU into low power mode and wait for an interrupt that a valid packet has been received to minimize current consumption. Transceivers from TI have digital output which generates an interrupt to the MCU if a packet has been received with OK CRC.