使用CCS9.0 import例程TIDA-010003,编译时总是报错Error: Program "make" not found in PATH。都是安装在默认目录。请问该如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用CCS9.0 import例程TIDA-010003,编译时总是报错Error: Program "make" not found in PATH。都是安装在默认目录。请问该如何解决?
Hi,Shi,感谢你的回复。按照你的指示,并把CCS9和simplelink_cc13x0_sdk_3_10_00_11的版本更换成TIDA-010003原有设定的CCS8和simplelink_cc13x0_sdk_2_40_00_20,目前如果set active为debug_poll,则编译通过并可以下载运行,但是如果设置为其余三个例如debug_push,则会报错。
error #10264: DEFAULT memory range overlaps existing memory range RAM
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "6lowpan_mesh_CC1310_LAUNCHXL_tirtos_ccs.out" not built
>> Compilation failure
makefile:272: recipe for target '6lowpan_mesh_CC1310_LAUNCHXL_tirtos_ccs.out' failed
gmake[1]: *** [6lowpan_mesh_CC1310_LAUNCHXL_tirtos_ccs.out] Error 1
makefile:268: recipe for target 'all' failed