This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310 UART Echo例程出现程序不运行的现象!



工具使用的是IAR,创建工程,导入TI-RTOS Examples中的UART Echo的例程。

问题:

1.在Debug模式下,在任务中设置断点,程序可以进入到echoFxn()任务中,在串口助手中也能打印调试信息

2.在运行模式下,程序则不进入echoFxn()任务中,串口助手没有任何调试信息。请问是什么原因?

以下为例程代码:主程序中点亮了一个灯,echoFxn()任务中去灭这个灯,这样更方便观察

请各位大佬帮忙解答,万分感谢!

/*
* ======== echoFxn ========
* Task for this function is created statically. See the project's .cfg file.
*/
Void echoFxn(UArg arg0, UArg arg1)
{
char input;
UART_Handle uart;
UART_Params uartParams;
const char echoPrompt[] = "\fEchoing characters:\r\n";

/* Create a UART with data processing off. */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_FULL;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.baudRate = 9600;
uart = UART_open(Board_UART0, &uartParams);

PIN_setOutputValue(ledPinHandle, Board_LED1, 0);
Task_sleep(333000/10);

if (uart == NULL) {echo
System_abort("Error opening the UART");
}


UART_write(uart, echoPrompt, sizeof(echoPrompt));

/* Loop forever echoing */
while (1) {
UART_read(uart, &input, 1);
UART_write(uart, &input, 1);
UART_write(uart, &input, 1);
}
}

/*
* ======== main ========
*/
int main(void)
{

Task_Params taskParams;

/* Call board init functions */
Board_initGeneral();
Board_initUART();

/* Construct BIOS objects */
Task_Params_init(&taskParams);
taskParams.stackSize = TASKSTACKSIZE;
taskParams.stack = &task0Stack;
Task_construct(&task0Struct, (Task_FuncPtr)echoFxn, &taskParams, NULL);

/* Open LED pins */
ledPinHandle = PIN_open(&ledPinState, ledPinTable);
if(!ledPinHandle) {
System_abort("Error initializing board LED pins\n");
}

PIN_setOutputValue(ledPinHandle, Board_LED1, 1);

/* This example has logging and many other debug capabilities enabled */
System_printf("This example does not attempt to minimize code or data "
"footprint\n");
System_flush();

System_printf("Starting the UART Echo example\nSystem provider is set to "
"SysMin. Halt the target to view any SysMin contents in "
"ROV.\n");
/* SysMin will only print to the console when you call flush or exit */
System_flush();

/* Start BIOS */
BIOS_start();

return (0);
}

  • 你好,multi task可以参考

    /*
     * Copyright (c) 2015-2019, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== mutex.c ========
     */
    
    /* XDC module Headers */
    #include <xdc/std.h>
    #include <xdc/runtime/System.h>
    
    /* BIOS module Headers */
    #include <ti/sysbios/BIOS.h>
    #include <ti/sysbios/knl/Clock.h>
    #include <ti/sysbios/knl/Task.h>
    #include <ti/sysbios/knl/Semaphore.h>
    
    #include <ti/drivers/Board.h>
    
    #define TASKSTACKSIZE   512
    
    Void task1Fxn(UArg arg0, UArg arg1);
    Void task2Fxn(UArg arg0, UArg arg1);
    
    Int resource = 0;
    Int finishCount = 0;
    UInt32 sleepTickCount;
    
    Task_Struct task1Struct, task2Struct;
    Char task1Stack[TASKSTACKSIZE], task2Stack[TASKSTACKSIZE];
    Semaphore_Struct semStruct;
    Semaphore_Handle semHandle;
    
    /*
     *  ======== main ========
     */
    int main()
    {
        /* Construct BIOS objects */
        Task_Params taskParams;
        Semaphore_Params semParams;
    
        /* Call driver init functions */
        Board_init();
    
        /* Construct writer/reader Task threads */
        Task_Params_init(&taskParams);
        taskParams.stackSize = TASKSTACKSIZE;
        taskParams.stack = &task1Stack;
        taskParams.priority = 1;
        Task_construct(&task1Struct, (Task_FuncPtr)task1Fxn, &taskParams, NULL);
    
        taskParams.stack = &task2Stack;
        taskParams.priority = 2;
        Task_construct(&task2Struct, (Task_FuncPtr)task2Fxn, &taskParams, NULL);
    
        /* Construct a Semaphore object to be use as a resource lock, inital count 1 */
        Semaphore_Params_init(&semParams);
        Semaphore_construct(&semStruct, 1, &semParams);
    
        /* Obtain instance handle */
        semHandle = Semaphore_handle(&semStruct);
    
        /* We want to sleep for 10000 microseconds */
        sleepTickCount = 10000 / Clock_tickPeriod;
    
        BIOS_start();    /* Does not return */
        return(0);
    }
    
    /*
     *  ======== task1Fxn ========
     */
    Void task1Fxn(UArg arg0, UArg arg1)
    {
        UInt32 time;
    
        for (;;) {
            System_printf("Running task1 function\n");
    
            if (Semaphore_getCount(semHandle) == 0) {
                System_printf("Sem blocked in task1\n");
            }
    
            /* Get access to resource */
            Semaphore_pend(semHandle, BIOS_WAIT_FOREVER);
    
            /* Do work by waiting for 2 system ticks to pass */
            time = Clock_getTicks();
            while (Clock_getTicks() <= (time + 1)) {
                ;
            }
    
            /* Do work on locked resource */
            resource += 1;
            /* Unlock resource */
    
            Semaphore_post(semHandle);
    
            Task_sleep(sleepTickCount);
        }
    }
    
    /*
     *  ======== task2Fxn ========
     */
    Void task2Fxn(UArg arg0, UArg arg1)
    {
        for (;;) {
            System_printf("Running task2 function\n");
    
            if (Semaphore_getCount(semHandle) == 0) {
                System_printf("Sem blocked in task2\n");
            }
    
            /* Get access to resource */
            Semaphore_pend(semHandle, BIOS_WAIT_FOREVER);
    
            /* Do work on locked resource */
            resource += 1;
            /* Unlock resource */
    
            Semaphore_post(semHandle);
    
            Task_sleep(sleepTickCount);
    
            finishCount++;
            if (finishCount == 5) {
                System_printf("Calling BIOS_exit from task2\n");
                BIOS_exit(0);
            }
        }
    }

    下面的 demo: