我在使用CC2500模块的时候,在多对一的RF系统中,为了避免发送时的冲撞,发送端需要先判断信道是否为空。但是我在调试了2个礼拜之后发现CCA的值一直不变cca = TI_CC_GDO2_PxIN & TI_CC_GDO2_PIN ; cca的值一直检测到为0。 所以我怀疑我的调试方法有误,希望使用过CCA功能的朋友,能给我指点下调试方法。如能有事例程序,那更加感激不尽。在此先行谢过各位!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用CC2500模块的时候,在多对一的RF系统中,为了避免发送时的冲撞,发送端需要先判断信道是否为空。但是我在调试了2个礼拜之后发现CCA的值一直不变cca = TI_CC_GDO2_PxIN & TI_CC_GDO2_PIN ; cca的值一直检测到为0。 所以我怀疑我的调试方法有误,希望使用过CCA功能的朋友,能给我指点下调试方法。如能有事例程序,那更加感激不尽。在此先行谢过各位!
http://www.ti.com/tool/simpliciti
下协议栈,直接看代码,里面有注释。想了解CCA,看数据手册。我附上这段代码吧。
这个函数支持非CCA直接发送和CCA判断再发送。
/**************************************************************************************************
* @fn MRFI_Transmit
*
* @brief Transmit a packet using CCA algorithm.
*
* @param pPacket - pointer to packet to transmit
* txType - FORCED or CCA
*
* @return Return code indicates success or failure of transmit:
* MRFI_TX_RESULT_SUCCESS - transmit succeeded
* MRFI_TX_RESULT_FAILED - transmit failed because CCA failed
**************************************************************************************************
*/
uint8_t MRFI_Transmit(mrfiPacket_t * pPacket, uint8_t txType)
{
#ifdef NWK_PLL
bspIState_t s;
#endif
uint8_t ccaRetries;
uint8_t returnValue = MRFI_TX_RESULT_SUCCESS;
/* radio must be awake to transmit */
MRFI_ASSERT( mrfiRadioState != MRFI_RADIO_STATE_OFF );
/* Turn off reciever. We can ignore/drop incoming packets during transmit. */
Mrfi_RxModeOff();
MRFI_PrepareToTx( pPacket );
/* ------------------------------------------------------------------
* Immediate transmit
* ---------------------
*/
if (txType == MRFI_TX_TYPE_FORCED)
{
//#ifdef NWK_PLL
// BSP_ENTER_CRITICAL_SECTION(s);
//#endif
// MRFI_CompleteTxPrep( pPacket );
#ifdef NWK_PLL
do
{
BSP_ENTER_CRITICAL_SECTION(s);
if( stx_active == false ) // if the channel was changed
{
BSP_EXIT_CRITICAL_SECTION(s);
Mrfi_RxModeOff(); // turn off the radio
MRFI_PrepareToTx( pPacket ); // setup transmission again
continue; // restart the loop
}
MRFI_CompleteTxPrep( pPacket );
} while( 0 );
#endif
/* Issue the TX strobe. */
mrfiSpiCmdStrobe( STX );
#ifdef NWK_PLL
BSP_EXIT_CRITICAL_SECTION(s);
#endif
/* Wait for transmit to complete */
Mrfi_DelayUsecLong( MRFI_MAX_TRANSMIT_TIME_us / 1000,
MRFI_MAX_TRANSMIT_TIME_us % 1000,
mrfi_TxImmediateDone );
/* Clear the interrupt flag */
MRFI_CLEAR_SYNC_PIN_INT_FLAG();
}
else
{
/* ------------------------------------------------------------------
* CCA transmit
* ---------------
*/
MRFI_ASSERT( txType == MRFI_TX_TYPE_CCA );
/* set number of CCA retries */
ccaRetries = MRFI_CCA_RETRIES;
/* For CCA algorithm, we need to know the transition from the RX state to
* the TX state. There is no need for SYNC signal in this logic. So we
* can re-configure the GDO_0 output from the radio to be PA_PD signal
* instead of the SYNC signal.
* Since both SYNC and PA_PD are used as falling edge interrupts, we
* don't need to reconfigure the MCU input.
*/
MRFI_CONFIG_GDO0_AS_PAPD_SIGNAL();
/* ===============================================================================
* Main Loop
* =============
*/
for (;;)
{
/* Radio must be in RX mode for CCA to happen.
* Otherwise it will transmit without CCA happening.
*/
/* Can not use the Mrfi_RxModeOn() function here since it turns on the
* Rx interrupt, which we don't want in this case.
*/
mrfiSpiCmdStrobe( SRX );
/* wait for the rssi to be valid. */
#ifdef MRFI_TIMER_ALWAYS_ACTIVE
MRFI_WaitTimeoutUsec(MRFI_RSSI_VALID_DELAY_US, Mrfi_ValidateRSSI);
#else // MRFI_TIMER_ALWAYS_ACTIVE
MRFI_RSSI_VALID_WAIT();
#endif // MRFI_TIMER_ALWAYS_ACTIVE
#ifdef NWK_PLL
BSP_ENTER_CRITICAL_SECTION(s);
if( stx_active == false ) // if the channel was changed
{
BSP_EXIT_CRITICAL_SECTION(s);
Mrfi_RxModeOff(); // turn off the radio
MRFI_PrepareToTx( pPacket ); // setup transmission again
continue; // restart the cca loop
}
MRFI_CompleteTxPrep( pPacket );
#endif
/*
* Clear the PA_PD pin interrupt flag. This flag, not the interrupt itself,
* is used to capture the transition that indicates a transmit was started.
* The pin level cannot be used to indicate transmit success as timing may
* prevent the transition from being detected. The interrupt latch captures
* the event regardless of timing.
*/
MRFI_CLEAR_PAPD_PIN_INT_FLAG();
/* Issue the TX strobe. */
mrfiSpiCmdStrobe( STX );
#ifdef NWK_PLL
BSP_EXIT_CRITICAL_SECTION(s);
#endif
/* Delay long enough for the PA_PD signal to indicate a
* successful transmit. This is the 250 XOSC periods
* (9.6 us for a 26 MHz crystal) See section 19.6 of 2500 datasheet.
* Found out that we need a delay of atleast 20 us on CC2500 and
* 25 us on CC1100 to see the PA_PD signal change.
*/
Mrfi_DelayUsec(25);
/* PA_PD signal goes from HIGH to LOW when going from RX state.
* This transition is trapped as a falling edge interrupt flag
* to indicate that CCA passed and the transmit has started.
*/
if (MRFI_PAPD_INT_FLAG_IS_SET())
{
/* ------------------------------------------------------------------
* Clear Channel Assessment passed.
* ----------------------------------
*/
/* Clear the PA_PD int flag */
MRFI_CLEAR_PAPD_PIN_INT_FLAG();
Mrfi_DelayUsecLong( MRFI_MAX_TRANSMIT_TIME_us / 1000,
MRFI_MAX_TRANSMIT_TIME_us % 1000,
mrfi_TxCCADone );
/* transmit done, break */
break;
}
else
{
/* ------------------------------------------------------------------
* Clear Channel Assessment failed.
* ----------------------------------
*/
/* Turn off radio and save some power during backoff */
/* NOTE: Can't use Mrfi_RxModeOff() - since it tries to update the
* sync signal status which we are not using during the TX operation.
*/
MRFI_STROBE_IDLE_AND_WAIT();
/* flush the receive FIFO of any residual data */
mrfiSpiCmdStrobe( SFRX );
/* Retry ? */
if (ccaRetries != 0)
{
#ifdef MRFI_TIMER_ALWAYS_ACTIVE
stx_active = false;
#endif
/* delay for a random number of backoffs */
Mrfi_RandomBackoffDelay();
MRFI_PrepareToTx( pPacket ); // setup transmission again
/* decrement CCA retries before loop continues */
ccaRetries--;
}
else /* No CCA retries are left, abort */
{
/* set return value for failed transmit and break */
returnValue = MRFI_TX_RESULT_FAILED;
break;
}
} /* CCA Failed */
} /* CCA loop */
}/* txType is CCA */
/* Done with TX. Clean up time... */
/* Radio is already in IDLE state */
#ifdef NWK_PLL
stx_active = false;
// Packet transmitted, regardless of packet type, remove reference.
sTxTimeStampAddr = NULL;
#endif
/*
* Flush the transmit FIFO. It must be flushed so that
* the next transmit can start with a clean slate.
*/
mrfiSpiCmdStrobe( SFTX );
/* Restore GDO_0 to be SYNC signal */
MRFI_CONFIG_GDO0_AS_SYNC_SIGNAL();
/* If the radio was in RX state when transmit was attempted,
* put it back to Rx On state.
*/
if(mrfiRadioState == MRFI_RADIO_STATE_RX)
{
Mrfi_RxModeOn();
}
return( returnValue );
}